Industry Online Support
Technical Forum
8/18/2012 11:50 AM | |
Joined: 12/11/2009 Last visit: 9/8/2022 Posts: 243 Rating:
|
Hello I worked with wincc many times but never worked with pcs7. We have a plant where scada system is pcs7,I have the step7 and wincc project ( or pcs7 project), I have to watch scada from my computer but I can't. I'm not sure if scada connects to plc or not.. I'm not even sure if pcs7 is updating tags or not. I'm adding a screen capture. can you watch and help me? Normally all the buttons must be active and my wincc starts to running I must see plant. But I see nothing. only grey screen. This is the original project, I copied from cd. Please helpppp Note: You need winrar to open file. When I normally zipped video it became 18mb and I could not upload it. When I zipped with winrar it became 3mb. but siemens forum does not accept rar file format. So Firstly I converted to rar file, then converted to zip file and it's still 3mb and zip file. Attachmentscreencapturepcs7_1 RAR.zip (77 Downloads) |
Follow us on