9/19/2012 8:54 AM | |
Joined: 2/20/2010 Last visit: 5/10/2024 Posts: 104 Rating: (7) |
Dear All, In one my site We have install PCS7 v 7.0 sp1 with one ES+OS and one OS station are running. Few day before i has add some I/O and do modification in CFC logic & compile OS program. After compiling project when start my Wincc Runtime at moment of Data manager loading Wincc RC PO Error message is coming. In that detail it showing that 412 tags present, limit is 2000. i coundn't understand why this error message is coming as I have already Wincc RC PO license of 2000 tags. after getting runtime this error message is coming frequently. I have recompile my OS complete still this error message is coming Is there any other reason... here I has attached Error message. Regards, Hitesh Attachmentscan0001.pdf (86 Downloads) |
9/19/2012 1:48 PM | |
Joined: 10/26/2011 Last visit: 6/12/2024 Posts: 762 Rating: (191) |
Hello could you send me the diagnose file from "C:\Program Files\SIEMENS\WINCC\Diagnose"? It seems, that you have to many variables or to many archive variables. It is displaey in the dignose file. |
SIMATIC PCS 7 - Overview |
|
9/19/2012 1:54 PM | |
Joined: 2/20/2010 Last visit: 5/10/2024 Posts: 104 Rating: (7) |
Hello, Please find attached diagnostics folder. AttachmentRe PCS7 Operator station and engg station problem.zip (92 Downloads) |
9/19/2012 3:13 PM | |
Joined: 10/26/2011 Last visit: 6/12/2024 Posts: 762 Rating: (191) |
In the sended Licsens_Info.log you can see, that you have to many archive variables. If you have no license for archive variables, you have 512 variables free. You have 521 archive variables in your project, that is the reason for the message. You have two posibilities: 1. reduce the archive variables equal or under 512 2. Buy the license for archive variables The smalles one ist for 1500 variables. Notice, you need this license for each runtime machine, in ypur case two licenses. I think, it is better to reduce your archive variables |
SIMATIC PCS 7 - Overview |
|
9/20/2012 8:42 AM | |
Joined: 2/20/2010 Last visit: 5/10/2024 Posts: 104 Rating: (7) |
Dear, Thanks for your reaply.. I got my Answer. |
Follow us on