3/6/2024 6:46 PM | |
Joined: 9/9/2015 Last visit: 9/4/2024 Posts: 727 Rating:
|
Hi, It seems that you have problem in downloading wincc application. I will explain the concept , hopefully it is helpful for you. Before downloading, you have to ensure 1. Your engineering station, OS Servers settings are correct. Run Security Controller to confirm. Start-> Siemens Automation -> Security controller-> Repeat settings. 2. Ensure the logon user has "SIMATIC HMI" right. For download, this is the main key role member you should assign to your user. 3. At the target host, for example, OS Servers, ensure you created a New folder, rename it with the name you want, right click properties -> sharing -> Advanced Sharing -> Share this folder, permissions-> ensure SIMATIC HMI has read/write access. At the next tab of folder properties, ensure Security has SIMATIC HMI read/write access. 4. At the ES, at the OS below wincc appl, right click and ensure the target host file can be "Browse". Try browse it and see. (You shouldd be able to ping via host name/computer name) 5. Then download OS.
|
Please give me 5 stars Rating if my post is helpful for you. :) |
|
3/9/2024 7:47 PM | |
Joined: 9/9/2015 Last visit: 9/4/2024 Posts: 727 Rating:
|
Hi Behnam, Thank you for the rating. Normally, if configuration is done properly, we do not require to change anything after download. Seem like you have executed the download process successfully from ES, then, you may check the load log by -> go to your os project , under wincc appl, right click OS -> display load log. The good OS download load log or process sequence should be 1. The project was locked 2. The entire WinCC Project will be transferred to the runtime OS 3. The target directory can be read and written to. 4. No project is open 5. The project was opened successfully. 6. The Picture tree was updated in xx:xx:xx. 7. Server data were created successfully. 8. The WinCC project is being closed. 9. The project was locked. 10. The computer name was changed in the project xxxx (Target Host name, If standby server, it will be named as the host name of standby server. Before changed, the computer name is ES host name). 11. The lock on the project was removed. 12. Downloading the OS in xx:xx:xx completed successfully. For your OS client, i believe your server data was not assigned correctly. To confirm 1. At your ES, under WinCC Appl Client , Right click the OS, Assign OS Server 2. If you see your server data is in black color with a tick in the right place, then it is fine. 3. If not, remove the tick in red color server data, press OK. 4. right click the OS again, assign server data, and reassign it to the correct server data. 5. perform an OS download again.(Before download, deactivate and close the target WinCC application manually, to make a smooth download) Hope it is helpful. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to
1 thankful Users |
Follow us on