10/6/2015 1:12 AM | |
Joined: 8/12/2011 Last visit: 4/27/2021 Posts: 65 Rating:
|
I am installing a WinCC Server Client app. I have it setup and tested in house under a workgroup. When I take this to the field, I need to convert it to a Redundant Domain Controller. Is there a document that can step me though the process? I have redundant OS Servers and 17 Clients. I do have Simatic Logon software and an extra license. I was told just need an license somewhere on the network to make it work or should it be on the domain controllers? The customer is providing the domain controllers and the Microsoft side of the set up. What do I have to do for the Siemens side of the set up once I am on site?
------------------------------------------------------------------------------------------ |
Last edited by: SMatthews at: 10/6/2015 1:13:07 AMLast edited by: Min_Moderator at: 10/6/2015 5:24:10 PMNew subject after splitting |
|
Follow us on