12/1/2020 7:13 PM | |
Joined: 9/23/2005 Last visit: 10/29/2024 Posts: 4351 Rating: (1451)
|
“Simple Samples” are small projects that demonstrate simple features. The target is give a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. Dynamic representations are a very important part of HMI / SCADA System. There are many elegant ways to show dynamic status, like Dynamic Widget, Text List, Graphic List, etc. Sometimes however what we need is just hide / show dynamically one object. It could be done using its “visible” property. It is possible to control the “visible” property linking it with a tag, using the system function “SetPropertyValue” or by Scripting. This Simple sample shows how to do it in these three ways. AttachmentHide.zip (1045 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to1 thankful Users |
Follow us on