9/8/2023 12:27 PM | |
Joined: 7/19/2022 Last visit: 6/13/2024 Posts: 364 Rating: (61) |
Hello Carlos_Mendes1, Yes, it is not tested or recommended to change the computer name after installing WinCC Unified RT PC. Especially if MS SQL is installed or used because the old PC name is linked to the SQL. You can try to start the “WinCC Unified Configuration” tool and the wizard makes the necessary settings That worked for me! |
If this Information really helps, you could use the Rate function |
|
9/8/2023 2:39 PM | |
Joined: 2/17/2020 Last visit: 6/14/2024 Posts: 1010 Rating: (178) |
Hi, Changing the name of the PC after installing WinCC SCADA (and here I include WinCC V7, WinCC Professional and WinCC Unified PC), can corrupt the installation and lose the link with the MS SQL Server that is installed with the software by default. From my experience, you can try uninstalling the software and SQL (please see this FAQ), running the Unified Configuration Tool again, but in many cases in the end the fastest and most effective solution is to start with a clean image of the operating system to install the software again and do not change the name of the PC again. Hope that helps. |
A rating will be well appreciated. |
|
9/8/2023 3:10 PM | |
Joined: 7/19/2022 Last visit: 6/13/2024 Posts: 364 Rating: (61) |
Hello again, I'm not sure if you will lose the old segments or not, but you have few other options. Use WinCC Unified Configuration or as @itafusna tells you, reinstall software and SQL. I have tried it only to rebind the SQL to the new PC name but I had no previous history. You can see in the attached video what the process would be like. AttachmentchangePCname.zip (274 Downloads) |
If this Information really helps, you could use the Rate function |
|
Follow us on