2/9/2018 12:32 PM | |
Joined: 3/14/2008 Last visit: 6/22/2024 Posts: 2071 Rating:
|
Hi Alex, First: Your OS: Windows 10 Enterprise x64 bit is not released for PCS7. It could be some of the rights are not correct....Even if it is set correctly, it can be blocked by Windows....especially with the Fall Creators update on Windows which messes up user rights... If it is a clean installation, I can only think that you have the wrong OS... |
If I could help you, you can use the RATE button. Thank you. |
|
2/9/2018 1:18 PM | |
Joined: 9/24/2015 Last visit: 5/8/2024 Posts: 79 Rating:
|
Hi Oerca Thank you for your answer ُSure installation is clean below link mentioned suitable OS https://support.industry.siemens.com/cs/ww/en/view/109745530 Operating systems SIMATIC PCS 7 V9.0 runs on the following operating systems:
but I did not pay attention to LTSB is it Problem ? |
Last edited by: Alex_BHP at: 2/9/2018 1:19:59 PMLast edited by: Jen_Moderator at: 2/12/2018 9:18:54 AMOptimized link. Alireza Rahaei |
|
2/9/2018 1:28 PM | |
Joined: 3/14/2008 Last visit: 6/22/2024 Posts: 2071 Rating:
|
Yeah.. LTSB (Long Term Servicing Branch). What it basically means is that you will not receive any big updates for the OS, no windows store, no Microsoft edge browser and is especially for PC's with must operate all the time in hospitals, automation and so on. You don't want the automation system crash because Microsoft changed something to the system. You will only receive critical security updates and patches. Whenever a new big update is released, Microsoft will release a new LTSB version-> At this moment there are two versions: 2014 and 2015. Only 2015 is released. When you want to be sure, please reinstall the system with a correct released Windows version. |
Last edited by: Oreca at: 2/9/2018 1:30:03 PMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
2 thankful Users |
10/9/2021 5:25 PM | |
Posts: 1 Rating:
|
I had the same issue. I fixed it by installing the latest updates/compatible software.
Please give me a rating if this post was helpful. :) Note: My opeating system is Windows 7 Ultimate SP1 Best regards CTRLSYS Team
|
Last edited by: Jen_Moderator at: 10/11/2021 11:32:18Optimized link. |
|
Follow us on