2/16/2009 6:09 AM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating: (1181) |
Hello Perhaps this manual would be helpfull: Compendium Motion Control (MC 1.66) There you can find Points to look out for when using certain option boards and CUMC ( Encoder interface connections TB, EB, CUMC boards) regards |
2/20/2009 10:38 AM | |
Joined: 3/29/2006 Last visit: 5/29/2017 Posts: 151 Rating: (8) |
The drive 6SE7136-5NJ62-3BA0-Z(Options:D10,D12,G91,K08,L55,L86,M05,M06,M21,M75,M76,M90 & S76) is a cabinet unit;Type: 6SE7036-5WK60 is a big Chassis II unit. The relevant compendium is this one http://support.automation.siemens.com/WW/view/en/13472409 All other drawings are copy-right of the company. For cabinet-units you can order some drawings. Please contact your next Siemens-office. |
2/21/2009 11:40 AM | |
Posts: 5 Rating: (0) |
Dear Sir, Can annybody in the forum provide me with some of the relevant drawings of the Inverter Secton? |
2/26/2009 2:21 PM | |
Posts: 101 Rating: (8) |
These documents are not readily available. They are a controlled document out of Germany and should only be available to service personel. |
Follow us on