7/22/2008 2:49 PM | |
Joined: 3/29/2006 Last visit: 5/29/2017 Posts: 151 Rating:
|
You can communicate with Masterdrives (change parameters, parameter-upload, - download) via Profibus (without CPU), if you - install DriveES Basic on the PC - have CommunicationBoardProfibus CBP2 in the drive http://support.automation.siemens.com/WW/view/en/27726644 http://www.siemens.com/drive-es --------------------------- Of course, this is also possible, if you have a Step7-CPU Routing from Ethernet to profibus is only possible via CPU. |
Follow us on