10/3/2016 8:47 PM | |
Joined: 4/2/2016 Last visit: 7/13/2022 Posts: 413 Rating:
|
video |
10/5/2016 10:07 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello _oleksandr_, Two alternates I would suggest you. 1. Which is the system for control of height adjustment of plasma & oxy fuel torch. Study the same & you can hard wire the interlocks to CNC controller which in turn disables drive. 2. Just install capacitive proximity switch on plasma & oxy fuel head bottom side & adjust the gap between switch & plate material in such a way that it must operate when the torch is about to hit plate material. Hard wire up this contact with CNC controller emergency switch input logic. HTH. |
Follow us on