7/11/2023 8:55 AM | |
Joined: 12/15/2016 Last visit: 5/15/2024 Posts: 56 Rating: (0) |
Sometimes I don't have internet even though I have the 3G modem correctly connected. I try to PING the internet and it doesn't respond. I connect a cable with a DHCP server to the P1 and then I already have PING on the internet. Then I disconnect the P1 cable and it does not change to take internet data through the 3G modem. I reboot without the P1 cable and at the 3G modem level everything remains the same, but now I do have internet. I insert the cable with DHCP server and I still have internet, then I take it out and switch and get the internet from the 3G modem. Everything is fine, but after a while you lose access to the internet again through the 3G modem. Do you know what is happening to me? I don't understand, has anyone had this happen to them and was able to fix it? Attached document with images. Thanks, Edu AttachmentProblema en el Modem.pdf (278 Downloads) |
7/24/2023 7:21 AM | |
Joined: 12/15/2016 Last visit: 5/15/2024 Posts: 56 Rating: (0) |
Hi Apastore, I thank you very much for answering me. I am looking forward to solving this problem. I can confirm that the IOT OS is V1.3.1. I am attaching a document with the correct connections. Maybe now nothing is visible to know the cause of the problem, but in the next few days when it fails I will send you the results with the connectivity problems. Yes, I'm sure it's not coming from the IOT, but I'd like to know where the error is coming from so I can attack the problem, but, I've already changed the 3G modem, antenna and SIM, I don't know what to do anymore. thank you very much.Attachmentsyslog.zip (278 Downloads) |
7/25/2023 1:13 PM | |
Joined: 12/15/2016 Last visit: 5/15/2024 Posts: 56 Rating: (0) |
Hi Apastore,
thank you very much. Attachment2.zip (265 Downloads) |
Last edited by: edurov at: 07/25/2023 13:16:59Last edited by: edurov at: 07/25/2023 13:19:57 |
|
Follow us on