3/20/2024 10:43 AM | |
Joined: 5/6/2022 Last visit: 9/12/2024 Posts: 442 Rating: (87) |
Hi AutoGen_2481162, It is true that it is sometimes difficult to retain so much information and to retain all that Siemens has to offer. In my case, what works best for me is to put everything I study into practice. The best way to learn, regardless of age, is to practice with it and stick with it because in the end you retain things much better when you have tried. In the end memorising is of little use. There are free online Sitrain courses from Siemens that can help! I encourage you to check them out. Best regards and cheers! |
If this Information really helps, you could use the Rate function |
|
Follow us on