8/17/2021 8:10 PM | |
Joined: 12/9/2020 Last visit: 10/19/2022 Posts: 46 Rating:
|
Yes |
8/17/2021 9:05 PM | |
Joined: 12/9/2020 Last visit: 10/19/2022 Posts: 46 Rating:
|
NO, i can't |
8/17/2021 9:06 PM | |
Joined: 12/9/2020 Last visit: 10/19/2022 Posts: 46 Rating:
|
I can't find publicAPI folder |
Last edited by: Fan_Mo at: 08/17/2021 21:13:53 |
|
8/18/2021 5:53 AM | |
Joined: 3/5/2017 Last visit: 8/21/2025 Posts: 780 Rating:
|
I have no idea why your registry is like it is, and i do not know if Openness is otherwise installed correctly. You can test if Openness works by adding registry entries yourself, Demo app will show and resolve the assemblies for certain, but if there is something else wrong besides entries, you might not be able connect to TIA. I'm pretty sure that those entries only contain info about assemblies and nothing else. Attached is a txt file, check file content and that the paths are correct (compare to my earlier pic), also that I have not made a file to screw up your registry. Change file to .reg, double click it and entries will be added. Or you can edit registry manually, like adding folders and files. File is for V16, but you can do same with other versions. PublicKeyToken is always the same. AttachmentV16.txt (740 Downloads) |
Last edited by: K_Ohjus at: 08/18/2021 05:55:34Last edited by: K_Ohjus at: 08/18/2021 05:56:21- Trying is the first step towards failure. |
|
This contribution was helpful to
3 thankful Users |
10/8/2021 11:07 PM | |
Joined: 8/15/2017 Last visit: 6/5/2023 Posts: 2 Rating:
|
James, thanks a lot! That solved my issue as well! Big big thanks :) |
4/26/2022 8:19 AM | |
Posts: 1 Rating:
|
Сonfirm, it solves the problem! |
8/1/2024 7:00 AM | |
Posts: 1 Rating:
|
disculpa cual fue el proceso que hciiste para q te funcione |
Follow us on