8/20/2009 2:40 PM | |
Joined: 1/4/2007 Last visit: 4/30/2024 Posts: 1112 Rating: (174)
|
Hello Sebastian_NLS, It is possible to calibrate the cells with the Siwarex JB. Please take a look into the following document: http://support.automation.siemens.com/WW/view/en/32467393 There you can find the calibrationinto the chapter 6.3 “Corner load adjustment”, especially the chapter 6.3.3 . The diference of 4 Wires or 6 Wires is: 4 Wires load cells have no Sense-wires, so you have to do a bridge into the JB between: - EXC+ and SEN+ - EXC- and SEN- Please see also into the document with the upper link the chapter 5.3 . The load cells with 6 wires need also resistors in the JB. You can connect to the Siwarex MS (S7-200) and the Siwarex U (S7-300) the same load cells (load cells with strain gauge principle). Best regards Siwarexi |
Follow us on