3/8/2011 8:50 AM | |
Joined: 10/7/2005 Last visit: 6/4/2024 Posts: 3008 Rating: (1051)
|
Hello GoForIT a couple of suggestion from my side to automatethe backup of onlineDB's are: 1.) Buy Versiondog (http://www.versiondog.com) or similar program. 2.) Build your own with the help of the command interface, have a look too at THIS and THIS forum post concenring it. |
Cheers |
|
This contribution was helpful to2 thankful Users |
3/27/2011 11:37 AM | |
Posts: 2 Rating: (0) |
Hi,GoForIT: I think the archive function of wincc can help you. Best regards.
|
3/28/2011 9:11 AM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359) |
Hi Please check the following post: indicating SFC82, SFC83 and SFC84 can be used to retain data? regards |
4/5/2011 9:19 PM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359) |
Why dont you use tag logging capability in WINCC.Data archiving is done automatically and it is olso possible to retrieve data for a specific time by using WINCC optional packages. WinCC/DataMonitorregards |
This contribution was helpful to1 thankful Users |
Follow us on