Industry Online Support
Technical Forum
7/6/2011 4:59 PM | |
Posts: 4 Rating:
|
Hi Phantom. I'm using Safety Matrix 6.2 on PCS 7 v7.1 SP2, WinCC v7.0 SP2 I'm able to monitor any Matrix from the ES. Whenever I try to open the matrices on any OS by clicking the block icon, I get an empty faceplate without any causes, effects or intersections. However if I click on any block icon belonging to a cause or effect, I am able to see case, intersections and effects. I also noticed that only on the matrices' block icons there is an "F" showing on the alarms area.
Splitted from Safety Matrix is empty on the OS. |
Last edited by: O_Moderator at: 7/7/2011 1:43 PMnew subject after splitting |
|
7/19/2011 6:39 AM | |
Posts: 13 Rating:
|
dear verbrennung The template files related to the F-systems are not updated in the latest version of PCS7. Please open all the F-related template file in your Os project and just save them. I think this should solve your problem. please post your findings... |
This contribution was helpful to
1 thankful Users |
Follow us on