4/8/2013 9:35 AM | |
Posts: 48 Rating: (0) |
Here you get my program, Like i said i get the time and date but i also need the day of the week. It should be simple but i'm not that good on 200
AttachmentClock.zip (143 Downloads) |
4/8/2013 11:03 AM | |
Posts: 37 Rating: (3) |
i don't know what VB7 should write to VB39 but it's wrong. VB39 it's used by HTA function on converting VB105 (seconds) to an ascii string.HTA function in your case uses 3 bytes (length 2), in the first byte is stored the length of the string and then are stored converted ascii characters. So when you use to convert to ascii and define length 2, and start byte VB39 you use VB39,VB40 and VB41. long story short replace in your program VB7 with VB107 and at OUTPUT write VB41 (not VB39).AttachmentClock with statuschart.zip (156 Downloads) |
Last edited by: adrian1982 at: 4/8/2013 11:36 AMI''''ve modify your prog and add a status chart to view your values. |
|
4/8/2013 11:38 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (713)
|
Hello, Your adressing was wrong indeed. Attached another working project, have a look at the Watch Table to see how your ascii characters are placed by the HCA instruction. Regards, Marcjan AttachmentClock_forum_ok.zip (171 Downloads) |
Last edited by: Marcjan at: 4/8/2013 11:44 AMProblem solved? |
|
4/9/2013 10:24 AM | |
Posts: 48 Rating: (0) |
I tried both programs but they didn't wiork. lets just say that my program is to get the pls to show me the: Time Date Day of the week
|
4/10/2013 10:30 AM | |
Posts: 48 Rating: (0) |
Finally I got it to work. Thank you for your help on this and your patience |
This contribution was helpful to1 thankful Users |
4/15/2013 10:11 AM | |
Posts: 48 Rating: (0) |
Thank you this was all I needed |
This contribution was helpful to1 thankful Users |
Follow us on