4/4/2013 7:20 AM | |
Posts: 48 Rating: (0) |
Hey I need helptoget the day of the week in to the pls,anyone that can help me?
|
4/4/2013 7:40 AM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (713)
|
Hello, I believe this FAQ makes things easy for you: How can you read out the S7-200 CPU clock and output the values in integer format and how can you set the S7-200 clock with default integer values? Regards, Marcjan |
Problem solved? |
|
This contribution was helpful to1 thankful Users |
4/4/2013 8:06 AM | |
Posts: 48 Rating: (0) |
Here you can see, vb107 is 0,it should 5. Got any ideas?
|
4/4/2013 9:37 AM | |
Posts: 461 Rating: (29) |
Hi, Post the set rtc & read rtc logic networks Regards, Nelliyan.G |
4/4/2013 9:53 AM | |
Posts: 48 Rating: (0) |
Here do you have READ_RTC. I do get the date and the time but i need to get the day of the week
|
4/4/2013 11:14 AM | |
Posts: 461 Rating: (29) |
Hi, I am not able to attach the code here so created in pdf , its working if u need code then provide mail id thr PM, i will fwd Hope it helps Regards, Nelliyan.G AttachmentRTC help.pdf (181 Downloads) |
Last edited by: Nelliyan randy at: 4/4/2013 11:14 AM |
|
4/5/2013 7:11 AM | |
Posts: 48 Rating: (0) |
I tried your program but it didnt work, its simple to get the date and the clock shouldnt it be simple to get the day of the week to? |
4/5/2013 8:31 AM | |
Posts: 461 Rating: (29) |
Hi VB157 carries the day of the week... Just now confirmed it in Image 1 at 23 H 48 M 12 S the vb 157 [day of the week ] was 4 In img 2 after 24 hrs, 00 h 00 m 05sec the vb157 takes the value 5 automatically.. My code is using 24:00 format.. Regards, Nelliyan.G AttachmentRTC help.pdf (174 Downloads) |
Last edited by: Nelliyan randy at: 4/5/2013 8:32 AM |
|
Follow us on