12/3/2011 12:17 AM | |
Posts: 5 Rating: (0) |
Hello all. I have a Simoreg drive for crane hoisting application, the drive is supply two different motion (Trolley motor & Jib motor with different specifications) , My problem is with jib lifting condition ,the drive is starting to lift the load but when the output current is reach to 290A (Motor rated current 230A) the alarm accrued(A031, A035 seriously ) and drive stop. I have trusted parameters list backup, I downloaded this parameters to the drive but there is no change, also I replaced the motor encoder & check the motor winding and brushes additional to all connections, I think the field current is normal but armature is not, plz help me… Is there problem with drive and hardware’s or motor? Notes: 1- This fault just happening with load lifting, however the drive working properly in case of load lowering! 2- When changing drive to the trolley motor motion there is no any problems. Attachment6ra70_3.pdf (181 Downloads) |
Last edited by: almoutaz at: 12/3/2011 12:21 AMLast edited by: almoutaz at: 12/3/2011 12:18 AM |
|
12/4/2011 5:47 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Can you attache drive parameter list here? |
12/4/2011 6:11 AM | |
Posts: 5 Rating: (0) |
Thank you for your interes..... I will do that... |
4/13/2014 10:49 PM | |
Joined: 9/1/2005 Last visit: 10/14/2024 Posts: 4109 Rating: (195) |
follow up question published by Rose Byrneis split to a seperate thread with the subject Install a small jib crane - bearing for the top pivot. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on