2/4/2007 11:55 AM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating:
|
Dear Gengus, Please download the handbook: DP/DP Coupler In the FAQ What are the special features of input/output addressing with the DP/DP coupler?you may find some extra information about the old and new DP/DP-coupler. For the programming it are two slaves that are independent are pprogrammed by the two masters. Different Baudrates are possible and also the possibility to "see" on the other side if the data is actual or that the other master not updating the data. The easiest way is to program on one side the outputs and on the other side the inputs and first look if that is working. With the dipswitches you may choose for the address and also if the first byte is used as statusbyte. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
2/4/2007 1:17 PM | |
Joined: 9/27/2006 Last visit: 1/17/2022 Posts: 62 Rating:
|
Late Thanks for your help on both problems. Gengus |
4/20/2015 10:35 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating:
|
|
Follow us on