6/18/2015 1:47 PM | |
Posts: 15 Rating: (0) |
Dear Expert, I want to set up a server/client network by wincc 7.3,I have one pc as a server and about 10 pcs as clients.I need to know is it possible to install windows 7 sp1 on server as an operation system and configure the network between server and other clients?I have heard that Win7 SP1 can just connect to 3 clients maximum and if we want to connect more than these number of clients we have to install windows server on server pc as an operation system?is it correct or not?please guide me by this network which OS I have to install on Server pc without having any problem to connect 10 clients?and if you have any documents regarding client/server configuration please share it. Regards, Iman
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 6/18/2015 2:48:45 PMNew subject after splitting |
|
6/18/2015 2:20 PM | |
Posts: 50 Rating: (3) |
Dear imanERC, There is a compatibility tool: I've never tried the tool though. I'm pretty sure you need serverOS if >3 clients. Janette |
6/19/2015 10:15 AM | |
Joined: 1/17/2006 Last visit: 4/16/2024 Posts: 800 Rating: (63) |
Yes you need 2008 on the server. Yes you can connect Win7 clients on this server for sure! |
6/19/2015 12:05 PM | |
Joined: 10/3/2010 Last visit: 4/25/2024 Posts: 1552 Rating: (188) |
Simply because Win 7 was not developed to be used as a server OS. It's architecture can't handle more. |
B r g d s , |
|
Follow us on