7/9/2012 3:51 PM | |
Joined: 3/7/2006 Last visit: 5/15/2024 Posts: 42 Rating: (7) |
Hello, i think would be excellent PID with DeadBand. This PID is very usefull, but DeadBand is very usefull in real life |
6/30/2013 1:43 PM | |
Posts: 113 Rating: (22) |
I had the same problem with LMN on Network 14 so I converted if from Input to InOut. I also had a problem because I don't use/install WinCC but I couldn't open PID Lean without it, so I temporarily added WinCC and have saved PID Lean as a Library, attached. I'm not at the office till Monday so I can't check that I haven't messed anything up till then.
AttachmentPIDLeanLibrary.zip (576 Downloads) |
This contribution was helpful to2 thankful Users |
7/11/2013 10:45 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Follow-up-question splitted to how calculate D Part in PID controllers? Best regards O_Moderator |
This contribution was helpful to1 thankful Users |
9/12/2013 2:15 PM | |
Joined: 9/1/2005 Last visit: 5/14/2024 Posts: 4101 Rating: (194) |
New question published by AmitCsplitted to Can we use PID Lean more than one time in a program? Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
8/31/2015 4:46 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
New question published by BMohsin is split to a separate thread with the subject PWM generation using Lean_PID. Best regards |
Follow us on