1/27/2015 12:02 PM | |
Joined: 7/6/2010 Last visit: 4/28/2024 Posts: 84 Rating: (1) |
Dear expert I have problem about ACB 3WL of Siemens. My project have 50 ACB connecto to PLC through Profibus network. PLC command on/off ACB and receive status on/off/trip through Profibus. PC Server use Wincc + Power rate software PLC 317- 2PN/DP Normal, I command on/off ACB ( in case ACB charge ok) and receive status on/off/trip throught Profibus is OK but my problem happen follow step : - Step 1 : PLC command on ACB through Profibus by bit 0/1 of byte n (in case ACB discharge) --> ACB fail close --> alarm display - Step 2 : I reset command on from PLC - Step 3 : After,I command on ACB again (in case ACB charge ok) but ACB can not receive command on from PLC. In case if i reset power supply for ACB immediately ACB receive command on from PLC and ACB is closed. So the reason why i reset power supply for ACB, ACB receive command on from PLC and ACB is closed ??? - Somebody show me bit reset ACB throught Profibus network - Pls help me explain parameter byte control ACB in attach file
AttachmentLV-WL_VL_circuit_breakers_PROFIBUS.pdf (228 Downloads) |
2/1/2015 3:27 PM | |
Joined: 7/6/2010 Last visit: 4/28/2024 Posts: 84 Rating: (1) |
Somebody help me pls |
9/5/2015 5:44 AM | |
Joined: 7/6/2010 Last visit: 4/28/2024 Posts: 84 Rating: (1) |
Dear expert please help me until now, my project sometime run somtime error |
Follow us on