11/28/2012 10:57 AM | |
Posts: 3037 Rating: (192)
|
Hello L.Rujoi, You should do the point 1.4 in the following link. What are the possible causes of an unsuccessful Microsoft SQL Server 2005 Express installation or why is creating or opening a WinCC flexible 2008 project aborted? Tweety |
11/29/2012 12:50 PM | |
Posts: 3037 Rating: (192)
|
Hello, you deinstall WinCC flexible after this you use the Clean up Support Tool. Now you install WinCC flexible again. What can cause the installation to abort or prevent successful starting of WinCC flexible? Tweety |
12/6/2012 12:53 PM | |
Posts: 3037 Rating: (192)
|
Hello, You can start a support request for your installation problem. ---> support request Tweety |
12/12/2012 3:29 PM | |
Joined: 11/15/2006 Last visit: 5/7/2021 Posts: 1319 Rating: (171) |
I think this is the best way. |
Have Fun! |
|
10/5/2016 1:54 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4768 Rating: (123) |
New question published by leomalex is split to a separate thread with the subject WinCC 2008 SP3 on Win7 32bit, stops when tring to install Microsoft SQP Server 2005. Best regards |
Follow us on