3/28/2017 8:01 AM | |
Posts: 215 Rating: (6) |
It should work with "db1,x0.0" instead of "db1,Bool0". |
This contribution was helpful to1 thankful Users |
3/30/2017 8:18 AM | |
Joined: 4/28/2015 Last visit: 4/30/2024 Posts: 3345 Rating: (377)
|
Hi karthikk, for this purpose you can use the Siemens IOT2000 Input/Output module. With this shield you have the possibility to send TWO digital outputs (24V) from your IOT to the S7-1200 CPU. If you want to have more outputs or outputs which are not boolean you can use i.e Modbus TCP to communicate. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
Follow us on