6/26/2017 10:13 AM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating:
|
Hi, On the first code you posted everything looks OK, except this line of code:
what you are doing here is setting the output of the timer block according to variable: "outTon" and the remaining time of the block is set by variable: "ET". It should be the other way around. Variable "outTon" and "ET" must be set according to "CYCLIC_TON.Q" and "CYCLIC_TON.ET" because the timer block is setting those outputs and you use those outputs to set your block outputs. Like this:
|
Last edited by: Oreca at: 6/26/2017 10:30:04 AMIf I could help you, you can use the RATE button. Thank you. |
|
6/28/2017 6:44 AM | |
Posts: 24 Rating:
|
Thank You alot Oreca. |
6/28/2017 6:56 AM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating:
|
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on