9/16/2017 11:32 AM | |
Joined: 12/18/2014 Last visit: 10/5/2024 Posts: 33881 Rating: (4214) |
Hello fahimjafry, please don't post twice or more. |
9/17/2017 2:19 PM | |
Joined: 9/27/2006 Last visit: 10/4/2024 Posts: 12283 Rating: (2685) |
Hello fahim; The backup you have for the WinCC Flexible contains the program, so you need to download WinCC Flexible 2008 (the only version available now is 2008 SP5) so you can restore the backup; therefore you need a computer ready and formatted to install the software, with one of different versions of Windows 7 or Windows 10; see the attached screenshot from the Compatibility tool, check with the information in the Servidce Pack 5 download link below. You can download the Trial version from the following link; the trial license is a working version of the software and will work for 14 days after installation, until you install the RT license: then it becomes fully functionnal. Delivery release: Service Pack 5 for SIMATIC WinCC flexible 2008 Compatibility Tool for Automation and Drive Technology For very basic informatiuon on WinCC Flexible 2008, see this Getting Started: SIMATIC HMI WinCC flexible 2008 Getting Started - First-Time Users As stated, you can work for 14 days with the trial version without limits, so you can start working with it immediately, restore your backup and prepare to install your communication link for Modbus TCP. Look at the dedicated chapter on Modicon processors in the following manual for details: SIMATIC HMI WinCC flexible 2008 Communication Part 2 Last, but important; you need to authoprize the software package so it becomes fully functionnal.This can be done at any time during the 14 days of the trial version. If you have any proof of ownership of the software (original USB key or license certificate, for example), Siemens will regenerate the license with a phone call if you start a Support Request (see the link at the top of this page). But you need the proof of ownership, either in your files or in possession of the contractors who programmed and installed this program (ask them...). This ALM software you can download here will let you see what Siemens licenses exist on your PC, and is the tool Siemens will use to regenerate the missing licenses. Hope this helps, |
Last edited by: dchartier at: 9/17/2017 2:25:25 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on