3/13/2018 7:27 AM | |
Posts: 69 Rating:
|
How can we apply brake using a PB DI BI? |
3/13/2018 7:51 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
In Sinamics DCM brake application is pre configured, only user need to define DO & connect corresponding BO to connect brake. Depending upon the type of brake, user need to activate the parameters which will take care of brake opening, closing operations interlinked with drive enable & motor running operation. e.g. P50080 = brake control mode, p50087 & 50088 br cntrl open & close time respectively. Please refer the attached sheet which explains the brake operation & its related parameter setting. (Extracted from Siemens manual) HTH. Attachment6RA80 Sinamics DCM brake application.pdf (250 Downloads) |
3/13/2018 8:14 AM | |
Posts: 69 Rating:
|
Ok! But can we use a PB to apply brake for slowing down the motor and when released going back to setpoint? |
3/14/2018 10:12 AM | |
Joined: 6/19/2017 Last visit: 6/21/2024 Posts: 8154 Rating:
|
New question published by Masru is split to a separate thread with the subject Explanation of hydraulic and pneumatic braking done through drive. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on