10/2/2017 2:34 PM | |
Joined: 4/11/2013 Last visit: 5/16/2024 Posts: 12 Rating:
|
Hello cuongaz80, The permanent self-monitoring feature of 3UG4625 ensures reliable system monitoring.The connected 3UL23 residual current transformer is also permanently monitored for open-circuit or short-circuit. The 3UL23 Transformer connecting cables must be twisted and not routed in parallel to live cables to protect from emitted interference. Keep the length of the connecting cables to a minimum.The resistance at the transformer connecting cable must not exceed 5Ωto ensure correct fault current monitoring. If you have furthermore the problem, please contact our Siemens Technical Assistance Support (technical-assistance@siemens.com). BR |
This contribution was helpful to
1 thankful Users |
Follow us on