(3)| 11/20/2020 9:34 AM | |
|
Joined: 9/30/2016 Last visit: 11/19/2025 Posts: 952 Rating:
|
Please also see the attached screenshots. I have a value (it originates from an encoder) that I compare to different values and when it gots close to one of the values it generate a short horn signal. I need to test some of the functionality with PLCSIM but how do I manipulate the value (in this case DB11.DBD62) to have values I want? I have tried a VAT but how do I manipulate from that? Will manipulating from VAT work as long as the logic in FC51 NW4 is writing 0 into DB11.DBD62 or do I need to disconnect that first? AttachmentEC1 meterhorn A.zip (580 Downloads) |
Follow us on