Industry Online Support
Technical Forum
11/6/2013 12:11 PM | |
Joined: 4/24/2006 Last visit: 9/23/2024 Posts: 8742 Rating: (1168)
|
Hello LouisO, Yes, this should be possible. The CPU151-8 can act as Profinet IO controller and Profinet I-device. You should in Hardware configuration of I-device go to PN-IO (double click) go to tab I-device Please select the option "I-device mode" and add the desired transfer area. When you are finished, please go to Options -> Create GSD file for I-device. Then you can import this GSD file into the Profinet IO controller. Perhaps this link might help: SIMATIC & SIMOTION: Configuring RT communication between SIMATIC and SIMOTION (I-Device) Best regards, Wizard |
11/6/2013 12:52 PM | |
Posts: 12 Rating: (0) |
Hi Thanks tried it and worked. |
This contribution was helpful to3 thankful Users |
Follow us on