1/31/2016 9:00 AM | |
Joined: 1/14/2016 Last visit: 3/23/2023 Posts: 29 Rating: (0) |
HI, I have the CPU 1212 and i want to ask what is the use of the 24 vdc out next to the supply of the cpu! |
1/31/2016 9:28 AM | |
Posts: 1529 Rating: (202) |
Just a convenient place to connect your input or output supplies. |
1/31/2016 10:13 AM | |
Joined: 1/14/2016 Last visit: 3/23/2023 Posts: 29 Rating: (0) |
In page 1133 of S7-1200 MANUAL it specificaly says that the current available (24VDC) IS 300mA max (sensor power)!!! |
2/5/2016 12:35 PM | |
Joined: 1/14/2016 Last visit: 3/23/2023 Posts: 29 Rating: (0) |
Should i fuse the 24VDC OUT? In case of a short circuit? And if yes 0.5A is ok since the maximum out is 0.3? |
Follow us on