2/6/2015 10:24 AM | |
Joined: 6/24/2013 Last visit: 10/7/2024 Posts: 1628 Rating: (421) |
Hello I have created a solution to the problem Function which converts Your meter output to double integer in kWh and a second integer in Wh for fractional part (changes from 0 to 999). You can display it as two boxes: XXXXXXXXXXX . YYY where xxxx is dint in kWh and yyy is int. the yyy must be displayed with leading 0s (like 015 not 15) and xxxxxx to be aligned to right; yyy aligned to left. the dot (.) is a static text. Attached: Project with solution How To Use: 1. Copy raw result from meter (Long Real, 8 bytes) into variable in DB1 2. call function (call exists in OB1) to convert to dint and int 3. copy results to variables used by HMI/SCADA AttachmentEnergy_meter_PAC3200.zip (291 Downloads) |
This contribution was helpful to2 thankful Users |
Follow us on