6/16/2019 11:35 AM | |
Joined: 4/2/2016 Last visit: 7/13/2022 Posts: 413 Rating:
|
3RQ30.. coupling relays with semiconductor output - switching voltage 110V DC? I'm looking coupling relays with semiconductor output with control supply voltage 24V DC switching voltage 110V DC (~ 0,1A). According to the catalog Siemens IC 10 · 2018 coupling relays 3RQ30.. has switching voltage max. 60V DC, but i need 110 V DC, which coupling relays (narrow design) with semiconductor output can i use? Something similar Phoenix Contact 2980678 SOLID-STATE RELAY MODULE PLC-OSC- 24DC/300DC/1, 6.2mm IN 24V DС; OUT 300V DC, 1NO, 1A. |
Follow us on