11/17/2015 2:03 PM | |
Joined: 6/7/2013 Last visit: 2/20/2024 Posts: 11 Rating: (0) |
Dear Tech. I have a ethernet network connected on 4 cpu s414, and then are connected on drivers (S120) by the profibus network, and my doubt is that I cannot connect on the driver by s7 online by ethernet cable. I have here on site cu 6sl3040-0la00-oaao (310-DP), I am configuring the driver by profibus connecting directly on the drive, I saw the manual to go online I made a lot of tests to try connection but nothing. I have some doubts about the version of the software in CU, if some version I cannot comunicate by S7 online, here on site is the version 2.5.x . I am using to connect Product: SCOUT Release: V4.4.0.4 thanks. everton vitti ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/18/2015 11:14:06 AMNew subject after splitting |
|
11/18/2015 1:10 PM | |
Joined: 6/7/2013 Last visit: 2/20/2024 Posts: 11 Rating: (0) |
Dear Chris. Follow some attached pictures how is configured my system to you understand better what is happen. 1 - About S7 online on Net Pro. - I asked to software guy here on site about it, and he aswear me that in another sites he didin't use this options and was working, so please can you send me more details about this configuration on Net Pro?. 2 - About try to connect online access - When I try show me the screen "Properties - Drives (Online)", and the tab modules the address to connect. (you can see the addres in the attached pictures). Thanks Everton Vitti. AttachmentS120.rar (219 Downloads) |
11/18/2015 7:09 PM | |
Joined: 6/7/2013 Last visit: 2/20/2024 Posts: 11 Rating: (0) |
Dear Dakine. Thanks for you answer, I changed together the software guy the sinamics GSD in the hardware configuration, was CU 320 DP, and on site I have CU 310 DP, but even that, it doesn't work, I have the same error, see attached pictures. I am connecting in the drive by the Pc Adapter cable directly on the profibus connector on the drive and the version of it is 2.5.x, only by ethernet (s7 online) I cannot connect. Best regards Everton Vitti. Attachments120_2.rar (167 Downloads) |
11/18/2015 7:18 PM | |
Joined: 6/7/2013 Last visit: 2/20/2024 Posts: 11 Rating: (0) |
Dear Chistop. Answer in bolded text. 1- why use 176.16.1.180 and then ping the 176.16.11.180 ? -Sorry my fault, I fix it and it isn't connecting. (same error). 2 - Why you use Rack 3 ? - Please confirm that I am using Rack 0 Slot 3, (see attached pictures). 3 - Don't use the object adress as Communication address ! - I fix it and it isn't connecting (same error) (Thanks for tip). Best Regards Everton Vitti. Attachments120_2.rar (165 Downloads) |
11/18/2015 8:19 PM | |
Joined: 6/7/2013 Last visit: 2/20/2024 Posts: 11 Rating: (0) |
Dear Christoph. See attached pictures that CPU is on the slot 3, please can you check in the attached pictures if the PG/PC config is ok?. I made the hardware modification but I cannot make download to CPU now because I have some mechanical guys working and I cannot stop the PLC. I started the accessible nodes and just show me the CPU's online and the IP's (see attached picture), It doesn't show me some "+" simbol on the Cpu's IP's. How you can see in the attached picture I am connecting in the PLC by the CP card. Thanks. Everton Vitti Attachments120_3.rar (171 Downloads) |
Follow us on