3/6/2014 12:47 PM | |
Joined: 1/28/2009 Last visit: 10/26/2024 Posts: 6852 Rating: (1365)
|
Hello, For better suggestions , we need the diagnostic buffer for the both CPUs.But still some points to be checked first:
Load the buffer for more information.Also check sections 5.1 and 5.3 of this manual. Best regards, Hamid Hosseini |
Last edited by: hdhosseini at: 3/6/2014 12:56 PM// TYPO |
|
3/10/2014 6:58 AM | |
Posts: 27 Rating: (0) |
Hello.....friend, |
3/11/2014 9:28 AM | |
Posts: 15 Rating: (0) |
Please find my design. 1) what the best time to switch the reserved H-CPU to RUN Mode? as most of the time when it is switch to RUN model we have reduncay Fault LED Red. 2) We have proble with the Commuction of X208 Switches? the commuction donst not work as per STAR toplogy? when one connector from Slave CPU is unpluged then it starts commuction but one switch has F LED continuously ON Thanks in advace. AttachmentRTC.pdf (460 Downloads) |
3/17/2014 6:15 AM | |
Posts: 15 Rating: (0) |
Thanks a lot for your reply. Pleas have a examiner view to my my design. i am facing problem with the sclcance x208 switch. we have star topology( is this toplogy ok as Star?). We want redundancy at each level. if we plug all the ports in switch( as per our design) we have then no communition and it seems that the switches does not support this configuration. if we have one port in TP900s ( instead of 2 ports as in our deisn) and 3 ports connection to PLC( instead of 4) then communtion goes ok, but with this we have BUS5F error in PLCs LED. Thanks in Advance. AttachmentRTC.pdf (375 Downloads) |
3/17/2014 6:46 AM | |
Posts: 515 Rating: (56) |
hi, did you assign any ip address for the two scalance X208 switch?
|
3/17/2014 7:11 AM | |
Posts: 15 Rating: (0) |
Yes sir we have assigned to 192.168.0.2 to S1 and 192.168.0.4 to S2. PLC1 192.168.0.5 PLC2 192.168.0.6 and 192.168.0.8 & 192.168.0.10 to TP900s. |
Follow us on