9/26/2022 7:07 AM | |
Posts: 1 Rating: (0) |
5SU1354-7KK16 Switching capacity : Switching capacity breaking capacity short-circuit current (Icn) / according to EN 61009-1 / rated value = 10kA switching capacity current ● according to EN 60898 / rated value 10 kA ● according to IEC 60947-2 / rated value 20 kA Which value should be used for an industrial sw.bd. Short circuit level for the sw.bd = 15 kA. Is the 5SU1354-7KK16 usable for this sw.bd ? Attachment5SU13547KK16_datasheet_en.pdf (517 Downloads) |
Follow us on