3/12/2013 7:00 PM | |
Joined: 9/27/2006 Last visit: 5/14/2024 Posts: 12257 Rating: (2668) |
Hello alifaez; The part number corresponds to a Simatic IPC, you are correct. WHat is important is what software you are running on the IPC. If you have a winAC RTX station, running Step 7, here are some links that could prove useful: WinAC RTX -- Configuring and programming communication -- Configuring connections how to upload from WinAC RTX v4.2 via Ethernet? |
3/13/2013 8:47 AM | |
Posts: 89 Rating: (7)
|
Hello! This product (see MLFB) belongs to a very old industrial PC (IPC), which is in the phase of discontinuation. (--> http://support.automation.siemens.com/WW/view/en/27581253). In general, just having an SIMATIC IPC does not meant, that you can download via Step7 a PLC programm. You have to install a so called software PLC, or softPLC, like the SIMATIC WinAC RTX (see links above). Only then this IPC can handle PLC tasks like a classical PLCs (e.g. S7-300). And one more hint: When you install the WinAC RTX (on any PC), you have to look into the library ofStep7and look for this WinAC RTX CPU, not for certain IPC. Only in the new TIA Portal - Step V12 you can find all currentthe SIMATIC IPCs directly. regards, moldi |
Last edited by: Moldi at: 3/13/2013 8:48 AM |
|
3/16/2013 12:09 AM | |
Joined: 9/27/2006 Last visit: 5/14/2024 Posts: 12257 Rating: (2668) |
Hello Ali-Mohammadi; I would presume the basic download and upload procedures for recent versions of WinAC RTX should be similar, although I have no direct experience with that particular version. You should find what you are looking for in the available documentation from Siemens: 6ES7671-0RC02-0YX0 SIMATIC WinAC RTX V3.1 Windows Automation Center WinAC RTX V3.1 Overview Hope this helps, |
Follow us on