11/20/2021 1:22 PM | |
Joined: 7/13/2013 Last visit: 12/10/2022 Posts: 23 Rating: (2) |
Hello Dear How can I find or download 6fc5 314-6cf00-0ab0 toolbox for Simatic Manager 5.5? Best regards |
11/20/2021 3:45 PM | |
Joined: 9/27/2006 Last visit: 4/27/2024 Posts: 12257 Rating: (2665) |
Hello karakas; The following link contis a link to the following Sinumerik document: NCU_060324_76.pdf https://support.industry.siemens.com/cs/ww/en/view/12620274 In this document, on page 7, 2 statements should attract your attention: "5.1 A new PLC based on the IBC16 chip has been has been developed with the NCU 572.4 / 573.4. The SINUMERIK order number for PLC 6FC5 314-6CF00-0AB0 corresponds to Simatic order number 6ES7 314-6CF00-0AB0" "5.3 PLC TOOLBOX: SINUMERIK components are now stored in a special "SINUMERIK" folder. In earlier versions, they are still stored in the "Rack 300" folder. You will need this toolbox to configure the NCU 573.4 as the hardware catalog for the PLC of the NCU 573.4 ( S7 PLC 314-C-2DP- 6CF00 ) has been modified" Since I am not very familiar with the SINUMERIK line of numeric controllers, I cannot provide much more help. It seems that the toolbox is integrated in the Sinumerik software on installation, and there are no download links available for the toolbox in Siemens links. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 11/20/2021 15:46:47 |
|
This contribution was helpful to1 thankful Users |
Follow us on