Industry Online Support
Technical Forum
11/15/2013 2:32 PM | |
Posts: 34 Rating: (2) |
Dear guys When I power on at first Simotion leds looks normal while booting. But at the end of start up phase all leds start to flash in red. No problem with CF card because it works with other D425. You can also find system log attached. AttachmentSYSLOG.pdf (339 Downloads) |
11/15/2013 2:49 PM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
Hello, in the BCD Segment is a E. or A. or F. ? Then it ist a SW defect in the SIMOTION FW. Regards Christoph |
11/18/2013 7:00 AM | |
Posts: 34 Rating: (2) |
There is "A" on BCD. Is there any way to solve this problem? |
11/18/2013 7:29 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
Hi, A. means asserttion in the FW. Which Version do you use? Regards Christoph |
11/18/2013 7:41 AM | |
Posts: 34 Rating: (2) |
Firm ware version is D4xx_V43SP1HF1_S120_V26SP2HF13 |
Follow us on