4/22/2016 9:00 AM | |
Posts: 62 Rating: (0) |
Hello, We have turning maschine 840dsl with 3 axis x z and sp. The spindle is DC motor with ADI4 nad they have 4 gears i have a problem with gear change betwen execution of program. When i wont to facing a piece from 300 fi to fi 0. I put the cconstant speed in m/min. So that mean when i start facing on fi 300 fi is speed in rpm about 100, when i finishing in fi 0 is speed about 1500rpm. I want that machine before operation change to 4 gear, because now is start with gear 1 and they stop operation when they rache 450rpm(max speed in gear 1). Can somebody give me advice how to resolve this problem. p.s. sorry for my english. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/22/2016 2:43:36 PMNew subject after splitting |
|
4/22/2016 9:16 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Why are you creating multiple posts for same problem? Please read reply here. |
4/22/2016 2:44 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
|
Follow us on