8/4/2008 6:25 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (306) |
Hello, For the 432-4U1x, the input filter (known as delay) is selectable between 3 msec , 1 msec and 0,3msec (via switch S5 on the board). For S7-300 for instance, several SM (signal modules) are available. You have for instance a so called "high speed" SM321 (SM 321; DI 16 x DC 24 V High Speed; (6ES7321-1BH10-0AA0), where the delay is less than 75µsec. Digital input module SM 321; DI 16 x 24 VDC; with hardware and diagnostics interrupts (6ES7321-7BH01-0AB0)
|
Best regards |
|
8/5/2008 8:04 AM | |
Posts: 767 Rating: (69) |
thanks for your kind reply, best regards. |
7/22/2013 3:12 PM | |
Joined: 3/2/2007 Last visit: 4/26/2024 Posts: 929 Rating: (5) |
which module is the best replacement for the6ES5432-4UA12 ? thank you |
... thank you ... |
|
Follow us on