11/22/2021 9:44 AM | |
Joined: 11/4/2011 Last visit: 9/20/2024 Posts: 233 Rating: (26) |
In the TO parameters you configure a system of units, which is then also used for these values. |
11/23/2021 8:12 AM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804) |
Hello, The acceleration is set accordingly as the position/s² unit of measure. The jerk is set accordingly as the position/s² unit of measure. 3.2.2 Units of measure The set units are displayed in the tag structure of the technology object <TO>.Units. The tag structure is described in the Appendix (Page 539) under the tags of the respective technology object. https://support.industry.siemens.com/cs/de/en/view/109749263 |
With best regards, |
|
Follow us on