7/1/2017 1:46 PM | |
Joined: 12/18/2014 Last visit: 5/6/2024 Posts: 32971 Rating: (4076)
|
Take a look at attachment.
AttachmentLOGO! 8 Soft manual 0BA8 2016_07 (FS4) pages 69-71.pdf (252 Downloads) |
7/1/2017 2:26 PM | |
Joined: 12/18/2014 Last visit: 5/6/2024 Posts: 32971 Rating: (4076)
|
If the message "Failed to submit" is displayed, the TDE has no connection to the LOGO!. And if the TDE doesn't has connect to the LOGO!, how should it then can Change settings in the LOGO! ? You have to enter in the LOGO! Selection menu of the TDE the IP address of the LOGO!, so that the TDE knows what address it is to connect to the LOGO!. AttachmentLOGO! 8 Soft manual 0BA8 2016_07 (FS4) page 353.pdf (160 Downloads) |
Last edited by: ixo65 at: 7/1/2017 2:43:49 PM |
|
7/1/2017 2:35 PM | |
Posts: 22 Rating: (0) |
great thanks. i have done it. |
This contribution was helpful to1 thankful Users |
Follow us on