8/30/2020 12:52 PM | |
Joined: 12/16/2018 Last visit: 6/16/2024 Posts: 67 Rating: (0) |
Hi AttachmentAttachments.zip (98 Downloads) |
8/31/2020 7:13 AM | |
Joined: 3/14/2008 Last visit: 7/11/2024 Posts: 2075 Rating: (930)
|
Hi DPCS, Thank you for including the installed software and image of the steps you have taken. That makes it easier to determine the issue. I think I know what is going on. The channel output drivers have a feature bit (Bit 30) that will determine the output value when a simulation signal is detected. Default setting is 1: Bit = 0: If process value input has the status 16#60, the output value will be set to the input value. Bit = 1: If process value input has the status 16#60, the output value will be set to “0”. So, please set bit 30 to FALSE and see if that solves the issue. When you place an AND block in between, you are basically elimination the signal status value in the structure, only the "Value" is transferred. In this case, the signal status is set automatically to 16#80, indicating a "good" value. PS: I notice in the installed software you have installed the following classic libraries: - SIMATIC PCS 7 Library V7.1+SP3+Upd2 - SIMATIC PCS 7 Faceplates V7.1+SP3 I suggest you will installed the latest updates for them as this is recommended (Better support for x64 systems and more). The library is not updated anymore (replaced by APL), but at least you are running the latest updates: - PCS 7 Library: V7.1+SP3+Upd4 - PCS 7 Faceplates: V7.1+SP3+Upd1 See Link under bullet 6 to download them. Best regards, |
Last edited by: Oreca at: 08/31/2020 07:20:48If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
9/3/2020 7:55 PM | |
Joined: 12/16/2018 Last visit: 6/16/2024 Posts: 67 Rating: (0) |
Hello Mr. oreca thank you very much The problem was solved with the help of your valuable and very useful tips Good luck
|
9/3/2020 10:21 PM | |
Joined: 3/14/2008 Last visit: 7/11/2024 Posts: 2075 Rating: (930)
|
Thank you for the feedback and good that your problem is solved |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on