8/24/2014 5:51 PM | |
Posts: 5225 Rating: (1185) |
Hi Michael. (GENERAL NOTE) This question is related to the software and not the S7-1200 PLC. It would do better in the STEP 7 (TIA Portal) conference. You are welcome to press the "Inform Moderator" button and ask that the post be moved there. (ANSWER TO QUESTION) The manuafacturers that supply Profibus (DP) and Profinet (PN) certified devices also supply a hardward description file. For profibus it is called a GSD file and Profinet has another "name". You should be able to get that file from the manufacturer which will make it possible for you to add the device in the catalog. You will not be able to program it with TIA, but you will be able to select some network capabilities so that your PLC knows how to communicate with the new device. The settings you set inside TIA should be replicated in the physical device too. You will not be able to transmit the TIA information into the device using TIA. There are a whole discussion that can follow, but i recommend you first see if you can find the GSD file and the documentation relating to that. Helpful? w |
This contribution was helpful to2 thankful Users |
8/24/2014 6:02 PM | |
Posts: 90 Rating: (0) |
Got It ... Thanks much.. I'll go to LinMot |
8/25/2014 12:01 AM | |
Posts: 5225 Rating: (1185) |
..okay |
This contribution was helpful to1 thankful Users |
8/25/2014 12:21 AM | |
Posts: 90 Rating: (0) |
By the way.. that's an aqwesome description of how to install it... Thanks again... |
Follow us on