11/11/2021 4:35 PM | |
Posts: 1 Rating: (0) |
I generated plccode to S7 simatic manger from matlab for traffic_light,of three lights now i want to simulate the code, but in DB there are allot of addresses which generated automatically and for simulation i think addresses of outputs must be the same with addresses of hardware of CPU313C, which the inputs of hardware from 124 to 126 and outputs from 142 to 125 . please help me, i this problem in my final project. T999.zip is the file of program, i want to implement the experience in reality for the graduation project, please help AttachmentT999.zip (272 Downloads) |
12/16/2021 3:58 PM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (133) |
Hello Albasety, for simulation with PLCSIM the address must not be the same by hwconfig and by the hardware. You can adjust the addresses later, if you work with the real CPU. And you can program the DB addresses or DB variables independently. See also the information of the FAQ: What are the essential differences between STEP 7 Lite and STEP 7 / STEP 7 Professional? With best regards |
Follow us on