2/21/2018 2:31 PM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928)
|
Hi, the best way to do this is by connecting the Interlock block output (inverted) to the motor external message 01, 02 or 03. You have three external messages which you can use. Open the motor block and go to mesages, now you can set the message type and comment for the external message. When triggered, your motor block tagname is displayed in the message and the group display is showing an alarm at the motor tag, so you know instantly were the interlock is triggered. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on