Industry Online Support
Technical Forum
7/31/2013 8:40 AM | |
Posts: 84 Rating: (19) |
KTP series of touch screens do not have a internal clock. So to have a real time clock I refer theEntry ID:39182145How do you synchronize the time of the HMI Basic Panel with an S7-1200 PLC? Now i am able to sync the PLC time and can display the real time over KTP, But when when any alarm triger, over the alarm log its all the default system time of KTP which start from year 2004. I have changed the "time_system_READ" tag to Cyclic continuous from cyclic operation. But still no change. Please help me to make all alarm log time same as HMI time which sync with S7-1200 PLC. I here by attached the TIA project file for reference. Thank you.
AttachmentS71200RnD.zip (209 Downloads) |
8/15/2013 8:09 AM | |
Posts: 84 Rating: (19) |
ThanksWizard, It works now. |
This contribution was helpful to1 thankful Users |
3/14/2014 1:19 PM | |
Joined: 10/23/2012 Last visit: 7/16/2023 Posts: 39 Rating: (0) |
please help me out from this issue alarm time is not same with the hmi time why? |
3/14/2014 1:24 PM | |
Joined: 4/24/2006 Last visit: 5/8/2024 Posts: 8638 Rating: (1151) |
Hello jkt_2, Have you seen this link: how do you synchronize the time of the HMI Basic Panel with an S7-1200 PLC? Best regards, Wizard |
Follow us on