7/2/2007 12:48 PM | |
Joined: 7/2/2007 Last visit: 6/18/2009 Posts: 2 Rating: (0) |
Hi We have problem with WinCC alarms that are strikethrough, and we can not acknowledge those messages. We are runnnig PCS7 v6.1 WinCC HF13 with redundant serverpair. We do not have this checkmark, that are mention in this support http://support.automation.siemens.com/WW/view/en/21378784 and the alarm are not locked/unlocked. Problem seems to accur when you take a way a block in the CFC and same block has an alarm in the WinCC. When we compile and download it do not disapear in WinCC RT. We can not stop both server at the same time. We can not delete runtime database. We have tried total download with memory reset. We have thetried unlock/lock meassages. Are there a simpel suolotion on this problem? Best Regards Peer95 |
7/2/2007 4:11 PM | |
Posts: 1776 Rating: (95)
|
Hi, do find this FAQ: http://support.automation.siemens.com/WW/view/en/17298206 maybe that explains. April |
7/3/2007 9:28 AM | |
Joined: 7/2/2007 Last visit: 6/18/2009 Posts: 2 Rating: (0) |
Nopp, the FAQ you are talking about are replaced with that oneI meanation |
7/4/2007 1:10 PM | |
Posts: 1776 Rating: (95)
|
Hi, so I know, You have no possibillity to remove this message. April |
12/12/2018 11:27 AM | |
Joined: 4/17/2018 Last visit: 1/4/2024 Posts: 1 Rating: (0) |
We recently have the exact same issue, is there already a solution for this? |
12/14/2018 1:53 PM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello StenB, the date and time of a message are shown crossed-out, if the message in the automation system is already due while starting the process execution of the operator station. Date and time do not correspond with the date and time at which the message in the automation system resulted. For more information see the manual SIMATIC Process control system PCS 7 OS process control (V9.0 SP1) in section Structure and States of Messages. And Siemenes offers a FAQ to delete non-acknowledgeable messages in the PCS 7 OS Runtime. But workaround is only for PSC 7 V9.0. With regards |
Follow us on